Dear Sir,
My product is based on TMS 43xx microprocessor with Linux OS on it meant for HMI interface with LCD display
It needs to receive information from the other subsystem using CAN BUS. Totally 5 nodes are present in the CAN Bus.
As long as as a single message transmissin and reception it is working perfectly.
when there are multiple messages , using socket CAN, the frames are not getting received. What could be the reasons?
How to set right this issue? Do you have any sample program or project based on Linux os? pl forward it.
I am badly struck . But the unit hangs when we handle the multiple CAN messages
And also attached the current IGCDU Qt project file also.
Pl send some sample code
Warm Regards,
S.M.Sundari
.