Im using IWR6843ISK with MMWAVEICBOOST, i download https://dev.ti.com/tirex/explore/node?node=AOVWxEvg-HcESecamNaaLg__VLyFKFf__LATEST this packge to use the RADAR in ros then i launched this file
roslaunch ti_mmwave_rospkg 6843_multi_2d_0.launch,
this is the information of the topic
rostopic echo /ti_mmwave/radar_scan
header:
seq: 688
stamp:
secs: 1625651852
nsecs: 195743514
frame_id: "/ti_mmwave_0"
point_id: 5
x: 6.54830789566
y: 3.18597197533
z: 0.0
range: 0.0
velocity: 0.0
doppler_bin: 0
bearing: 0.0
intensity: 0.0
I want to know if this topic provide the distances and the angle to detect obstacles, if the response yes where is the information and finally why the range in the topic every time is zero?