Hi team,
Customer wants to use LMX8410L and they want to achieve below.
RF input frequency = LO input frequency, then, they want to get IF output frequency = DC.
Now they have questions about mixing spurs that is explained on 3.6 of the app note, snaa329.
2x2 spur = the mixed signal of the second RF harmonic and the second LO harmonic
3x3 spur = the mixed signal of the third RF harmonic and the third LO harmonic
1x1 spur : F1 + F1=2×F1 --- (1) Undesired Signal
F1 - F1=0=DC1 --- (2) Desired Signal
2x2 spur : 2×F1 + 2×F1=4×F1 ---(3) Undesired Signal
2×F1 - 2×F1=0=DC2 ---(4) Undesired Signal
3x3 spur : 3×F1 + 3×F1=6×F1 --- (5) Undesired Signal
3×F1 - 3×F1=0=DC3 --- (6) Undesired Signal
Q3. If Q2's understanding is correct, does 2x2 spur that is described on 3.6 mean equation (2)? And 3x3 spur that is described on 3.6 mean equation (5)?
And if this understanding is correct, can the sentence on 3.6 as below and figure 8&9 be proven by equation (2)&(3)?
"In fact, the mixing spurs from the LMX8410L are almost negligible."
Q4. How should they understand equation (4) & (5)? (4) & (5) are DC and they are not sure whether they should understand these as mixing spurs.