Other Parts Discussed in Thread: AFE7444
Hi ,
I want to increase the AFE ref clock to 384 MHz. I tried it, but Internal VCO seems to be not tuned properly. I make 16x interpolation and the Clockout of AFE is not 2.048GHz.
As per theory, it should be 384*16 = 6.144 GHz ( DAC Clock) and ADC clock = DAC clock/3 = 2.048 GHz. This should be the same as Clock out of AFE.
Can you please let me know if it is possible to do that in AFE7444 EVM?
Right Now I am programming LMK of AFE with Prescaler 5 and M value at 5 so the VCO Freq will be 3.072 GHz. Then I divide it by 8 to get the AFE REF clock to 384 MHz.
Please help me in this regard if possible.
With regards,
Ganesh Singh