Other Parts Discussed in Thread: USB2ANY, LMX8410L
Dear community,
I am working with the board LMX8410LEVM and have to configurate the in an internal LO mode over SPI.
I see on the oscilloscope, that MOSI work, but MISO do not. All data on MISO are zero. When I try to read the default value of register, I receive only zeros on MISO canal.
I use the user guide, from to configure and to enable MUXout canal, register R0[2] = 0, to enable reading on MOXout(MISO) canal .
Can you tell me, what I do wrong?
Best Regards,
Iordan Pentchev.