I plan to use four single ended GPIOs - one for TX_4CH_TDD, one for RX_4CH_TDD, one for ADC_4ch_SYNC_IN, and one for DAC_4ch_SYNC_OUT.
Can I select any GPIO or is there any recommended pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I plan to use four single ended GPIOs - one for TX_4CH_TDD, one for RX_4CH_TDD, one for ADC_4ch_SYNC_IN, and one for DAC_4ch_SYNC_OUT.
Can I select any GPIO or is there any recommended pin?
Hi Yoonsun,
Preferred balls for TXA_TDD, RXA_TDD, CMOS ADC_SYNC0 and CMOS DAC_SYNC0 are H15, E7, H8 and H9 respectively.
Below parameter can be set to control all 4 Tx and 4 Rx channels' TDD with TXA_TDD and RXA_TDD respectively.
sysParams.modeTdd = 0
To use common sync (SYNC0) for all Rx channels, set below parameter:
sysParams.rxJesdTxSyncMux= [0,0,0,0]
To use common sync (SYNC0) for all Tx channels, set below parameter:
sysParams.jesdRxSyncMux = [0,0,0,0]
To configure single-ended or CMOS SYNC, set below parameters:
sysParams.jesdABLvdsSync = 0
sysParams.jesdCDLvdsSync = 0
All the system parameters and GPIO configuration are explained in AFE79xx_ConfigurationGuide_SBAA417_Jun2020.pdf available on secure folder.
Regards,
Vijay