Other Parts Discussed in Thread: LMK04828, LMX2582, LMX2594
Hello,
I am following the User Guide (SLAU706A) for TSW40RF8x Evaluation Module.
I am specifically repeating Section 3 (Basic Set-Up) and Section 4 (Quick Start Procedure).
I have checked everything is connected and signals are as per Section 3.2. But as I click 'LOAD DEFAULT' in the TSW40RF8x EVM GUI, I get the 'Device Initialization Error' popup pasted below.
I don't know what (1) and (2) mean as they are not indicated in the Test Set-up Block Diagram in Figure 2. I have ensure that (3) is done. But I still get this error.
Also, I have reviewed the schematic for the EVM and made sure other jumpers are in the positions indicated as in the schematic names JP3 (shunt 1 and 2), JP7 (shunt 1 and 2), JP8 (shunt 1 and 2), JP6 (shunt).
Any advice would be greatly appreciated.
I