Dear TI experts,
I'm trying to get the AFE7900EVM up and running, together with a TSW14J56 capture card. I followed the instructions listed in the SBAU338_EVM_UG_Version_1.pdf, and AFE79XX_Latte_UserGuide.pdf, but I can't get it to work.
I'm running these scripts in Latte in the following sequence:
-setup.py
-devInit.py
- any AFE79xx_EVM_ModeX.py -> leads to an error window: Unable to read Firmware Version. Check clock and supplies to A...
I attached the console output as well as the Latte Log.
Do you have any information on how to solve this ?
Thank you
#====== #Executing .. AFE79xx/bringup/setup.py #Start Time 2022-08-09 17:27:56.355000 AFE79xxLibraryPG1p0 spi - USB Instrument created. resetDevice Purge MPSSE mode set Kintex RegProgrammer - USB Instrument created. Kintex RegProgrammer - USB Instrument created. Kintex RegProgrammer - USB Instrument created. #Done executing .. AFE79xx/bringup/setup.py #End Time 2022-08-09 17:28:03.402000 #Execution Time = 7.04699993134 s #================ ERRORS:0, WARNINGS:0 ================# #====== #Executing .. AFE79xx/bringup/devInit.py #Start Time 2022-08-09 17:28:11.648000 Power Card - USB Instrument created. Reset the FPGA and try again. Loaded Libraries #Done executing .. AFE79xx/bringup/devInit.py #End Time 2022-08-09 17:28:37.593000 #Execution Time = 25.9449999332 s #================ ERRORS:1, WARNINGS:0 ================# #====== #Executing .. AFE79xx/bringup/AFE79xx_EVM_Mode2.py #Start Time 2022-08-09 17:28:59.159000 The External Sysref Frequency should be an integer factor of: 3.84MHz 2T2R1F Number: 0 Valid Configuration: True laneRateRx: 9830.4 laneRateFb: 9830.4 laneRateTx: 9830.4 2T2R1F Number: 1 Valid Configuration: True laneRateRx: 9830.4 laneRateFb: 9830.4 laneRateTx: 9830.4 Device Initialization for ChipVersion: 2.0 DONOT_OPEN_Atharv_FULL - Device registers reset. chipType: 0xa chipId: 0x78 chipVersion: 0x20 LMK Clock Divider - Device registers reset. LMK Clock Divider - Device registers reset. REFCLOCK is used from LMK source, ensure board connections are ok to do the same SPIA has got control of PLL pages PLL Pages SPI control relinquished. Fuse farm load autoload done successful No autload error Waiting for MACRO_DONE bit to go high, Count: 1 Waiting for MACRO_DONE bit to go high, Count: 2 Waiting for MACRO_DONE bit to go high failed Execution stopped #Done executing .. AFE79xx/bringup/AFE79xx_EVM_Mode2.py # End Time 2022-08-09 17:29:50.503000 # Execution Time = 51.3440001011 s #=======================================
[18120] PyInstaller Bootloader 3.x [18120] LOADER: executable is C:\Program Files\Texas Instruments\Latte\bin\latte.exe [18120] LOADER: homepath is C:\Program Files\Texas Instruments\Latte\bin [18120] LOADER: _MEIPASS2 is NULL [18120] LOADER: archivename is C:\Program Files\Texas Instruments\Latte\bin\latte.exe [18120] LOADER: No need to extract files to run; setting extractionpath to homepath [18120] LOADER: SetDllDirectory(C:\Program Files\Texas Instruments\Latte\bin) [18120] LOADER: Already in the child - running user's code. [18120] LOADER: Python library: C:\Program Files\Texas Instruments\Latte\bin\python27.dll [18120] LOADER: Loaded functions from Python library. [18120] LOADER: Manipulating environment (sys.path, sys.prefix) [18120] LOADER: sys.prefix is C:\PROGRA~1\TEXASI~1\Latte\bin [18120] LOADER: Setting runtime options [18120] LOADER: Initializing python [18120] LOADER: Overriding Python's sys.path [18120] LOADER: Post-init sys.path is C:\Program Files\Texas Instruments\Latte\bin [18120] LOADER: Setting sys.argv [18120] LOADER: setting sys._MEIPASS [18120] LOADER: importing modules from CArchive [18120] LOADER: extracted struct [18120] LOADER: callfunction returned... [18120] LOADER: extracted pyimod01_os_path [18120] LOADER: callfunction returned... [18120] LOADER: extracted pyimod02_archive [18120] LOADER: callfunction returned... [18120] LOADER: extracted pyimod03_importers [18120] LOADER: callfunction returned... [18120] LOADER: Installing PYZ archive with Python modules. [18120] LOADER: PYZ archive: latte [18120] LOADER: Running pyiboot01_bootstrap.py [18120] LOADER: Running pyi_rth_mplconfig.py [18120] LOADER: Running pyi_rth_mpldata.py [18120] LOADER: Running pyi_rth_multiprocessing.py [18120] LOADER: Running pyi_rth_pkgres.py [18120] LOADER: Running pyi_rth_win32comgenpy.py [18120] LOADER: Running pyi_rth__tkinter.py [18120] LOADER: Running pyi_rth_qt4plugins.py Qt: Untested Windows version 10.0 detected! [18120] LOADER: Running latteExec.py <string>:151: SyntaxWarning: import * only allowed at module level Connecting... 0 ERROR: Please check environment setup! No device is detected. FTDI Not Connected Instantiated: Class lmkLib Instantiated: Class fpgaLib_J58 Instantiated: Class RRFLib Instantiated: Class RxDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class RxDDCLib Instantiated: Class RxDGCLib Instantiated: Class RxFbILCLib Instantiated: Class RxDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class RxDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class RxDDCLib Instantiated: Class RxDGCLib Instantiated: Class RxFbILCLib Instantiated: Class RxDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class FbDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class FbDDCLib Instantiated: Class FbDGCLib Instantiated: Class RxFbILCLib Instantiated: Class FbDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class RRFCalibConfig Instantiated: Class TTLib Instantiated: Class TxDigLib Instantiated: Class TxDigLib Instantiated: Class RRFLib Instantiated: Class RxDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class RxDDCLib Instantiated: Class RxDGCLib Instantiated: Class RxFbILCLib Instantiated: Class RxDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class RxDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class RxDDCLib Instantiated: Class RxDGCLib Instantiated: Class RxFbILCLib Instantiated: Class RxDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class FbDigLib Instantiated: Class ALCLib Instantiated: Class AGCLib Instantiated: Class FbDDCLib Instantiated: Class FbDGCLib Instantiated: Class RxFbILCLib Instantiated: Class FbDSAGPEC Instantiated: Class RxDCCorrLib Instantiated: Class RRFCalibConfig Instantiated: Class TTLib Instantiated: Class TxDigLib Instantiated: Class TxDigLib Instantiated: Class DsaLib Instantiated: Class TopProcLib Instantiated: Class DProc1Lib Instantiated: Class DProc1FwDbgLib Instantiated: Class DProc1AggrHwLib Instantiated: Class DProc1MailboxLib Instantiated: Class TopLib Instantiated: Class pllLib Instantiated: Class TimingController Instantiated: Class IoWrapLib Entered: getAllFunctions of class IoWrapLib Entered: getAllFunctions of class IoWrapLib Instantiated: Class JESDLib Instantiated: Class DACJesdLib Instantiated: Class DACJesdLib Instantiated: Class ADCJesdLib Instantiated: Class ADCJesdLib Instantiated: Class serdesLib Instantiated: Class serdesLib Instantiated: Class jesdSubchipLib Instantiated: Class MacroLib Instantiated: Class CalibTopHw Entered: initializeConfig of class afe78xxLibrary Entered: findFactorX of class afe78xxLibrary Entered: fcwAutoConversion of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: checkValidityOfDigChain of class afe78xxLibrary Entered: initializePllConfig of class afe78xxLibrary Entered: initializeSerdesConfig of class afe78xxLibrary Entered: initializeGpioConfig of class afe78xxLibrary Instantiated: Class cpldLib Entered: initializeConfig of class afe78xxLibrary Entered: findFactorX of class afe78xxLibrary Entered: fcwAutoConversion of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: checkValidityOfDigChain of class afe78xxLibrary Entered: initializePllConfig of class afe78xxLibrary Entered: initializeSerdesConfig of class afe78xxLibrary Entered: initializeGpioConfig of class afe78xxLibrary Entered: initializeConfig of class afe78xxLibrary Entered: findFactorX of class afe78xxLibrary Entered: fcwAutoConversion of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: checkValidityOfDigChain of class afe78xxLibrary Entered: initializePllConfig of class afe78xxLibrary Entered: initializeSerdesConfig of class afe78xxLibrary Entered: initializeGpioConfig of class afe78xxLibrary Entered: deviceBringup of class afe78xxLibrary Entered: initializeConfig of class afe78xxLibrary Entered: findFactorX of class afe78xxLibrary Entered: fcwAutoConversion of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: findJesdClockDivFactors of class afe78xxLibrary Entered: getAdcDataMuxValues of class afe78xxLibrary Entered: customAdcDataMux of class afe78xxLibrary Entered: checkValidityOfDigChain of class afe78xxLibrary Entered: initializePllConfig of class afe78xxLibrary Entered: initializeSerdesConfig of class afe78xxLibrary Entered: initializeGpioConfig of class afe78xxLibrary Entered: softReset of class afe78xxLibrary Entered: deviceSoftReset of class afe78xxLibrary Writing into 0x0000 value 0x30 Writing into 0x0000 value 0xb0 Writing into 0x0000 value 0x30 Writing into 0x0000 value 0x30 Writing into 0x0000 value 0x30 Reading From 0x0003 value 0x0a Reading From 0x0004 value 0x78 Reading From 0x0005 value 0x00 Reading From 0x0006 value 0x20 Reading From 0x0007 value 0x51 Reading From 0x0008 value 0x04 Entered: lmkConfig of class lmkLib Entered: lmkPllConfig of class lmkLib Entered: lmkSysrefEn of class lmkLib Entered: configureFpgaJesd of class afe78xxLibrary Entered: reset of class fpgaLib_J58 Entered: checkVersion of class fpgaLib_J58 Entered: getCaptureSettings of class afe78xxLibrary Entered: fpgaTxConfig of class fpgaLib_J58 Entered: getCaptureSettings of class afe78xxLibrary Entered: getCaptureSettings of class afe78xxLibrary Entered: selectDrive of class fpgaLib_J58 Entered: getCaptureSettings of class afe78xxLibrary Entered: fpgaRxConfig of class fpgaLib_J58 Entered: selectCapture of class fpgaLib_J58 Entered: wakeupDevice of class afe78xxLibrary Writing into 0x0015 value 0x80 Writing into 0x0191 value 0x00 Writing into 0x0231 value 0x00 Writing into 0x02d1 value 0x00 Writing into 0x0371 value 0x00 Writing into 0x042a value 0x00 Writing into 0x04e2 value 0x00 Writing into 0x059a value 0x00 Writing into 0x0652 value 0x00 Writing into 0x070a value 0x00 Writing into 0x07c2 value 0x00 Entered: overrideTdd of class TopLib Writing into 0x00ec value 0x01 Writing into 0x00f4 value 0x01 Writing into 0x00e4 value 0x01 Writing into 0x00ed value 0x00 Writing into 0x00f5 value 0x00 Writing into 0x00e5 value 0x00 Writing into 0x0015 value 0x00 Writing into 0x0015 value 0x40 Writing into 0x0190 value 0x03 Writing into 0x0190 value 0x01 Writing into 0x0015 value 0x00 Entered: delay of class afe78xxLibrary Entered: setCm4Div of class TopLib Writing into 0x0015 value 0x02 Writing into 0x00c0 value 0x00 Entered: setClockTermination of class afe78xxLibrary Entered: requestPllSpiAccess of class TopLib Writing into 0x0015 value 0x00 Writing into 0x0015 value 0x40 Writing into 0x0170 value 0x01 Writing into 0x0540 value 0x00 Entered: logPoll of class TopLib Reading From 0x0171 value 0x01 Writing into 0x0015 value 0x00 Writing into 0x0015 value 0x01 Writing into 0x0054 value 0x81 Writing into 0x0015 value 0x00 Entered: requestPllSpiAccess of class TopLib Writing into 0x0015 value 0x40 Writing into 0x0170 value 0x00 Writing into 0x0540 value 0x00 Entered: delay of class TopLib Writing into 0x0015 value 0x00 Entered: reloadEfuseChain of class TopLib Writing into 0x0015 value 0x40 Writing into 0x08a8 value 0x02 Writing into 0x0810 value 0x01 Writing into 0x0830 value 0x01 Writing into 0x0200 value 0x00 Writing into 0x0210 value 0x00 Writing into 0x0814 value 0x00 Writing into 0x0834 value 0x00 Writing into 0x0814 value 0x01 Writing into 0x0834 value 0x01 Writing into 0x0810 value 0x00 Writing into 0x0830 value 0x00 Writing into 0x0810 value 0x01 Writing into 0x0830 value 0x01 Writing into 0x0200 value 0x05 Writing into 0x0210 value 0x00 Writing into 0x0814 value 0x03 Writing into 0x0834 value 0x03 Writing into 0x0814 value 0x00 Writing into 0x0834 value 0x00 Writing into 0x0810 value 0x00 Writing into 0x0830 value 0x00 Writing into 0x0814 value 0x00 Writing into 0x0834 value 0x00 Writing into 0x0814 value 0x1c Writing into 0x0834 value 0x1c Writing into 0x0814 value 0x00 Writing into 0x0834 value 0x00 Entered: delay of class TopLib Entered: checkEfuse of class TopLib Reading From 0x0150 value 0x0f Reading From 0x0150 value 0x0f Entered: enableEfuseClock of class TopLib Writing into 0x0830 value 0x01 Writing into 0x0810 value 0x01 Writing into 0x0910 value 0x0f Writing into 0x0911 value 0x03 Writing into 0x0912 value 0x0f Writing into 0x0015 value 0x00 Entered: resetTopProc of class TopProcLib Writing into 0x0018 value 0x20 Writing into 0x0140 value 0x01 Entered: resetTopProc of class TopProcLib Writing into 0x0140 value 0x00 Entered: delay of class afe78xxLibrary Entered: getFwVersion of class MacroLib Reading From 0x00f0 value 0x01 Entered: logPoll of class MacroLib Writing into 0x00a3 value 0x00 Writing into 0x00a2 value 0x00 Writing into 0x00a1 value 0x00 Writing into 0x00a0 value 0x02 Writing into 0x0193 value 0x01 Entered: delay of class MacroLib Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f1 value 0x00 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f0 value 0x01 Reading From 0x00f3 value 0x00 Reading From 0x00f2 value 0x00 Reading From 0x00f7 value 0x00 Reading From 0x00f6 value 0x00 Reading From 0x00f5 value 0x00 Reading From 0x00f4 value 0x00 Reading From 0x00fb value 0x00 Reading From 0x00fa value 0x00 Reading From 0x00f9 value 0x00 Reading From 0x00f8 value 0x00 Reading From 0x00ff value 0x00 Reading From 0x00fe value 0x00 Reading From 0x00fd value 0x00 Reading From 0x00fc value 0x00