Other Parts Discussed in Thread: TRF370417
Hi Team,
The TRF3705 IQ modulator datasheet states that its 1-dB input frequency bandwidth is 1000MHz. Does this IQ modulator output RF signal with a bandwidth of up to 2000MHz?
Thanks,
Annie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hsia,
The data sheet of TRF370417 IQ modulator also states that its 1-dB input frequency bandwidth is 1000MHz. However, in section 7.3 of the data sheet, it is stated that a 2GHz bandwidth RF signal can be generated using the full baseband bandwidth. Customer would like to know how to understand it?
Thanks,
Annie
Yes, the TRF3705 supports a baseband bandwidth of 1 GHz corresponding to an RF BW of 2 GHz. The baseband I/Q (in-phase and quadrature-phase) paths each support ~0Hz to 1 GHz. When those paths are combined in the modulator and up-converted by the LO, you will get double the baseband bandwidth. The output RF spectrum will be LO +/- 1 GHz for a composite 2 GHz total bandwidth.
--RJH
Hi RJH,
Does the baseband I/Q path support negative frequencies? For example -500MHz to 500MHz band, the center frequency is 0Hz?
Thanks,
Annie
Hi RJH,
May I ask how the baseband I/Q of TRF3705 is combined, and can double the baseband bandwidth when upconverted by the LO? Or is the output RF bandwidth of the IQ modulator always 2x the I/Q baseband bandwidth?
Thanks,
Annie
Hi Annie,
Typically, with the direct upconversion with message signal m(t) and Hilbert transform mh(t) of bandwidth B, your final upconverted signal will have 2*B of total bandwidth. Below is the generic equation for most of the I/Q modulators.