This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF371125EVM USB Control

Other Parts Discussed in Thread: TRF371125, TSW3003

Hello,

 

I have 2 TRF371125 mixer eval boards that I am using in a system. I am using TI's provided software to program the two boards via USB, however, when I have both boards connected to the same PC, I am only able to program one of the boards and not the other. Moreover, I do not know which board is being programmed since the software does not give any indication of the serial number, etc. Is there any solution for this? Also, can you provide the source code for the programming interface of these boards?

Thanks,
Neema 

  • Neema,

    This problem is similar to using multiple TSW3003.  The USB interfaces were never designed to be used for putting together multiple boards in a system.  They were geared for evaluation of a one EVM at a time and as such there were no provisions put in place to handle multiple EVMs using the same PC.

    Regards,

    Ken.