Other Parts Discussed in Thread: AFE7686,
I want to use DAC Jesd mode (L_M_F_S_HD 1TX = 22210x24 HBW).
The datasheet says that the mode (22210x24 HBW ) is available, but "Register Programming for JESD and Interpolation Mode" doesn't have a value for that item.
According to the "register set Manual", the following calculation was applied, but a Jesd configuration error occurred.
JESD_MODE(B"01011"),
JESD_PHASE_MODE(B"11")
CLKJESD_DIV(B"101")
CLKJESD_OUT_DIV(B"110")
INTERP_FRONT(B"010")
INTERP_BACK(B"1")
This value is the value that worked normally in the previous AFE7686.
I hope for your help in this regard.
thank you