Other Parts Discussed in Thread: AFE7900EVM
Hi,
I am designing a custom board using AFE7906 and have the below query,
1) Since AFE7906 has only RX and no TX, is SYNCB-OUT connection to FPGA required?
2) What is the purpose of JTAG pins and how should i connect ? can i perform Boundary scan using on board FPGA or external device?
3) In DC135A_AFE7900EVM, 27uF feed-through capacitor is used to isolate multiple rails ( VOUT_1p8V_CLK and VDDA_GPIO_1p8 ). How to calculate the Rejection offered by the feed-through? Is it better to use a ferrite instead of this to increase PSRR/Isolation?
4) In DC135A_AFE7900EVM, VDDA1P8 and VDD1P8GPIO are shorted together. can i power this using a Buck convertor or an LDO is mandatory?
Awaiting your reply at the earliest.
Thanks in-advance,
Deva