Other Parts Discussed in Thread: AFE8000
Hi,
I've noticed that there are values differences of caps & inductors on the AFE8000EVM board matching network:
For example -
* (RXA_IN, J26) C410 equals 0.7pF, L76 equals 2.8nH, C409 = 1.3pF etc
* (RXB_IN, J4) C34 equals 1.2pF, L15 equals 1nH, C35 = 1.7nH etc

What is the reason for these differences?
Is it due to the EVB layout, to compatible to the AFE8000's relevant input (1RXIN vs 2RXIN)?
Best regards,
Avihay.