Part Number: AFE7953
Other Parts Discussed in Thread: AFE7950, AFE7950EVM
We are using AFE7953EVM module in our design. We do not have FTDI chip in our design so we can not control the AFE7953 directly with Latte Software. We want to program the AFE registers directly with FPGA via SPI interface without Latte software.
In our earlier experiment with AFE7950 development board, Latte software was generating latte_log.txt (attached with this email) for python script latte_code.txt(attached with this email). We were using latte_log.txt to write the programming sequence within FPGA.
We observed that, when development board is not connected to PC then the latte log file was not generating.
Our queries are,
- Is there a way to generate register log file (equivalent to latte_log.txt) with Latte software without connecting to AFE development board(we do not have AFE7953 development board)?
- We have register set generated for AFE7950(Latte log with development board), can we use the registers sequence directly with AFE7953?
Please help us with above queries.
Regards,
Obul.
############## Read me ##############
#In HSDC Pro DAC tab, Select AFE79xx_2x2TX_14810; Data Rate = 122.88M
#In HSDC Pro ADC tab, Select AFE79xx_2x2RX_14810; Data Rate = 122.88M
sysParams=AFE.systemParams
sysParams.__init__();sysParams.chipVersion=chipVersion
setupParams.skipFpga = 1 # setup FPGA (TSW14J56) using HSDC Pro
############## Top Level ##############
sysParams.FRef = 491.52
sysParams.FadcRx = 2949.12
sysParams.FadcFb = 2949.12
sysParams.Fdac = 2949.12*4
sysParams.externalClockRx=False
sysParams.externalClockTx=False
sysParams.RRFMode = 0 # RRF 0: 4T4R2F FDD Mode
sysParams.enableDacInterleavedMode=False
############## Digital Chain ##############
##### RX #####
sysParams.ddcFactorRx = [24,24,24,24] #DDC decimation factor for RX A, B, C and D
sysParams.rxNco0 = [[4000,4000], #Band0, Band1 for RXA
[4000,4000], #Band0, Band1 for RXB
[4000,4000], #Band0, Band1 for RXC
[4000,4000]] #Band0, Band1 for RXD
##### FB #####
sysParams.ddcFactorFb = [6,6] #DDC decimation factor for FB 1 and 2
sysParams.fbNco0 = [4000,4000] #Band0 for FB1 and FB2
sysParams.fbEnable = [False,False]
##### TX #####
sysParams.ducFactorTx = [96,96,96,96] #DUC interpolation factor for TX A, B, C and D
sysParams.txNco0 = [[4000,4000], #Band0, Band1 for TXA
[4000,4000], #Band0, Band1 for TXB
[4000,4000], #Band0, Band1 for TXC
[4000,4000]] #Band0, Band1 for TXD
############## JESD ##############
##### ADC-JESD #####
sysParams.jesdSystemMode= [3,3]
#SystemMode 0: 2R1F-FDD ; rx1-rx2-fb -fb
#SystemMode 1: 1R1F-FDD ; rx -rx -fb -fb
#SystemMode 2: 2R-FDD ; rx1-rx1-rx2-rx2
#SystemMode 3: 1R ; rx -rx -rx -rx
#SystemMode 4: 1F ; fb -fb- fb -fb
#SystemMode 5: 1R1F-TDD ; rx/fb-rx/fb-rx/fb-rx/fb
sysParams.jesdTxProtocol= [0,0] # 0 - 8b/10b encoding; 2 - 64b/66b encoding
sysParams.LMFSHdRx = ["14810","14810","14810","14810"]
# The 2nd and 4th are valid only for jesdSystemMode values in (0,2).
# For other modes, select 4 converter modes for 1st and 3rd.
sysParams.LMFSHdFb = ["22210","22210"]
sysParams.rxJesdTxScr = [False,False,False,False]
sysParams.fbJesdTxScr = [True,True]
sysParams.rxJesdTxK = [8,8,8,8]
sysParams.fbJesdTxK = [8,8]
sysParams.jesdTxLaneMux = [7,1,2,3,6,5,4,0] # Enter which lanes you want in each location.
# For example, if you want to exchange the first two lines of each 2T,
# this should be [[1,0,2,3],[5,4,6,7]]
##### DAC-JESD #####
sysParams.jesdRxProtocol= [0,0]
sysParams.LMFSHdTx = ["14810","14810","14810","14810"]
sysParams.jesdRxLaneMux = [7,4,2,3,6,5,1,0] #[7,6,2,3,4,5,1,0] #0,1,2,3,4,5,6,7] # Enter which lanes you want in each location.
# For example, if you want to exchange the first two lines of each 2R
# this should be [[1,0,2,3],[5,4,6,7]]
sysParams.jesdRxRbd = [3, 3]
sysParams.jesdRxScr = [False,False,False,False]
sysParams.jesdRxK = [8, 8, 8, 8]
##### JESD Common #####
sysParams.jesdABLvdsSync= True
sysParams.jesdCDLvdsSync= True
sysParams.syncLoopBack = True #JESD Sync signal is connected to FPGA
############## GPIO ##############
sysParams.gpioMapping = {
'H8': 'ADC_SYNC0',
'H7': 'ADC_SYNC1',
'N8': 'ADC_SYNC2',
'N7': 'ADC_SYNC3',
'H9': 'DAC_SYNC0',
'G9': 'DAC_SYNC1',
'N9': 'DAC_SYNC2',
'P9': 'DAC_SYNC3',
'P14': 'GLOBAL_PDN',
'K14': 'FBABTDD',
'R6': 'FBCDTDD',
'H15': ['TXATDD','TXBTDD'],
'V5': ['TXCTDD','TXDTDD'],
'E7': ['RXATDD','RXBTDD'],
'R15': ['RXCTDD','RXDTDD']}
############## LMK Params ##############
lmkParams.pllEn = True
lmkParams.inputClk = 1474.56 # Valid only when lmkParams.pllEn = False
lmkParams.lmkFrefClk = True
setupParams.fpgaRefClk = 245.76 # Should be equal to LaneRate/40 for TSW14J56
############## Logging ##############
logDumpInst.setFileName(ASTERIX_DIR+DEVICES_DIR+r"\Afe79xxPg1_4000_obul2.txt")
logDumpInst.logFormat=0x01
logDumpInst.rewriteFile=1
logDumpInst.rewriteFileFormat4=1
device.optimizeWrites=0
device.rawWriteLogEn=1
device.delay_time = 0
#-------------------------------------------------------------------------------------------------#
#line 119 changes ps
sysParams.useSpiSysref=True
AFE.deviceBringup()
AFE.TOP.overrideTdd(15,3,15) # bit-wise; 4R,2F,4T