This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF87: Input sample rate is only up to 1.25GSPS???

Part Number: DAC38RF87

Tool/software:

Hello team,

My customer is confused with this device.

The table 9 shows that input sample rate for JESD204 is onyl up to 1250MSPS.

My customer would like to output 1GHz sine wave, so they want to input at least 2000MSPS to the DAC. (They want to operate the DAC in 4000MSPS)
Eventhough, it will be interpolated up to 7500MSPS, I am assuming the interpolation cannot increase the frequency of the output sine wave, interplation will only make the waveform smoother right?

Is it possible for this DAC to output 1GHz? I am afraid it can only output up to 625MHz sine wave... (1250MSPS / 2 = 625)

Best Regards,
Kei Kuwahara