Part Number: AFE7920
Tool/software:
We are using the Latte release with API version 2.5. Our system is based on a custom board integrating the AFE7920 and Xilinx JESD204B IP, with the JESD interface configured in 8B/10B mode. While the JESD link can eventually achieve link-up, we observe that performing the AFE initialization only once often results in the JESD link failing to come up. The link is typically established only after performing an AFE reset followed by a full reinitialization. However, this process introduces significant latency due to the long AFE initialization time.
No errors or warnings are observed during the AFE initialization process.
Is there a method to reliably bring up the JESD link without requiring multiple AFE resets and initializations?
and How can I read the temperature sensor of the AFE7920?