I have one board in a batch of 12 that has a problem with the LMX2531LQ1312, the only sign of a problem other than I do not get any frequency output from the Ic is that the "Vreg Buf" signal on pin 6 is low when it should have voltage on it.
I have checked this pin for short circuit to ground, had the board X-rayed and the chip replaced, still no joy.
The data sheet does not have enough information on it to detail why this signal might be low when all the other PSU pins with there decoupling caps are OK.
Is there a more detailed block diagram of the internals of this chip so I can work out what is causing this one board to fail?