Currently using the TRF370317 as a quadrature modulator with an advertised operating RF output from 400 to 4000 MHz. A customer requested RF output at 200 MHz. The TRF370417 has an advertised RF output from 50 to 6000 MHz, however, sideband supression is degraded down to 70 MHz according to the datasheet. IC swap from '317 to '417 shows that '317 has better amplitude imbalance and phase error at 200 MHz. That was a surprise! What steps are required to tune the circuit for use with a '417? What are the equivelent circuit models for '417 LO/IF/RF pins?
thanks,
B.May