Hello
I'm using two GC5016, one in 4 channels DDC mode and the other in 4 channels DUC mode. The parameters of my design are:
CK: 40MHz
Ftune: 10MHz
cic_dec: 64
fir_dec: 2
fir_int: 2
cic_int: 64
Everything is ok except the following: I'm using the gc5016_filterdesign MATLAB script to design DDC and DUC FIR filter taps. First of all, I use a delta for the DDC filter and design the filter for the DUC, and everything works as expected. When I design the filter taps for the DDC and load them into the GC5016 I found that, without input signal, there are three tones at 10MHz, 10.104MHz and 9.896MHz. I'm reviewing all the documentation and posts on this forum, but I can't find neither explanation or idea wich explains what is happening.
Please can you help me to solve this? I'm completely stopped at this point
Thanks in advance
Andres