Dear Sir \ Madam
In my design I need to phase compare 2 high frequency signals (2GHz).
I think of using the LMX2434 phase detector part and the divider part as follow :
the first signal go from the signal source (DDS synthesizer) to FinRF input (pin 15,16 of the LMX) directly.
the second signal gos from the same source trough a variable delay to the FinIF input (pin 3) prescaled & divided down to about 600 MHz
The signal from the IF 18 bit counter feed trough the MUX to Ftest output (pin 10) ( (pre programmed by the microcontroller)
The signal from the MUX out externally connected to OSCin (pin 8) and feed the phase detector trough the 15 bit R counter
The phase detector is programed to compare 2 20MHz signal
The DC voltage from the phase detector output should indicate the phase diffrance between the the 2 signals.
My question is : is this design can work?
Please see attached picture describing the design.6114.Phase detector.pdf