Hi,
I would like to do measurements based on the WiFi 802.11ac standard which requires a carrier frequency in the 5GHz band and a signal bandwidth of 80MHz.
Is it possible to generate such signals with the DAC3282EVM?
On the website http://www.ti.com/tool/dac3283evm it is stated that this evaluation module features the TRF3704 which is able to operate at 5GHz, but in the user guide, it is stated that the board comes with TRF3720 and TRF3703, which both are not able to operate at 5GHz. Could you tell me, which modulators are on this board?
Kind Regards,
Harald