Hi,
I'm brand new to this device, and this field in general. I am looking to use the TRF370417EVM to perform frequency modulation of a supplied carrier signal (434MHz) with IQ signals from a dual channel signal generator (likely ~160Hz sinusoidal signals 90deg out of phase with one another). This setup is just used to create a known test signal, which we want to confirm we can demodulate with the rest of our system.
In the SLWU062 document (March 2010), it indicates that an arbitrary waveform generator can be used to supply the I/Q signals. I'm hoping there is a very simple answer here, but how do I physically connect the signal generator output to the EVM board IQ inputs? The board has 4 x SMA connectors (I+, I-, Q+, Q-), and my signal generator (AFG3052C) only has 2 x BNC outputs at 50ohm.
I would appreciate your feedback.
Thank you,
Paul