Other Parts Discussed in Thread: ADS54J20
I downloaded the IBIS-AMI model for ADS58J63. I see two package model files in it namely - tx_package_DA0.s4p and tx_package_DA1.s4p.
I would like to know if these are the actual package models related to ADS58J63 or if it is some example mode.
Reason behind this query is I was refering to the user guide
ADS54J20_AMI_users_guide.pdf
Table 2 in this user guide list all the models included in the IBIS-AMI model. But this table doesn't list the package model files.
Hence request you to confirm if the included package model are the actual models which I can use for my simulation.
If not then request you to provide the same. This is required to carry out my SI analysis.
Regards,
Kiran