I need to know what is the number of effective bits at the serial output of this device when configured in all three fixed point modes (rounded 16-bits, rounded to 24 bits, and full 32-bit resolution) and using the set of filters included in the data sheet.
What is the improvement in the noise floor when moving from 16 to 24 to 32 bits?
Figure 60 suggests that although the coefficients are 16-bit, the output of the FIRs are 21-bits wide
Thank you