Part Number: ADC32RF80
hi, TI
If developers measure the case temperature and the board temperature,
do they obtain the junction temperature from the equation below?
Thanks and Best Regards,
OHTA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, RJH
Thank you for your reply.
I confirmed SPRA953C”Semiconductor and IC Package Thermal Metrics”.
It says that the equation(Equation 4) is invalid.
Also, SPRA953C says that Ψjt should not be used when application of a heat sink is intended. Instead, Equation 5 and Equation 6 should be used.
but, I cannot measure θsa. so, I cannot calculate the junction temp by Equation 5 or Equation 6.
For that reason, I deduced that equation( I thought that equation with the idea of a two-resistance model)
which equation should I use for calculating correct junction temperature?
Spra953c says that Equation 4 is invaild.
Because, a very small percentage of heat energy in a typical plastic package is convected and radiated off the top surface of the package.
Tj [degC] = Tc [degC] + theta-jc [degC/W] * Pdiss [W] _______Equation 4
So, I deduced a equation below with the idea of two-resistance model.