Other Parts Discussed in Thread: TRF370317
I find there is no description about the input Peak-Peak range.
Plz ,help me to find it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The nominal input swing to the I/Q ports is differential 1V peak-to-peak. You can check out Figure 1 in the TRF370317 datasheet which depicts the power output with respect to input swing (SE in the graph). The modulator portion of the TRF3702017 shares the same IP as the TRF370317.
--RJH