Team,
We are using the TRF3722 on another project and the team is having difficulty configuring the TRF3722 through the SPI bus. Could you provide a detailed step by step programming procedure?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
We are using the TRF3722 on another project and the team is having difficulty configuring the TRF3722 through the SPI bus. Could you provide a detailed step by step programming procedure?
If the issue is related to the SPI mechanics then section 7 in the datasheet offers a good picture on how to set up the SPI data, clock, and enable lines for programming.
If the issue is how to determine the register values, then section 8 in the datasheet provides the formulas to calculate the required divider ratios. The TRF3722 GUI is also good resource to use to observe/verify device register settings are matching expectations.
The GUI will write registers 1-6 excluding register 2 and then write that one last. Register 2 triggers the auto-cal bit and should be toggled once the other registers have been solidified. Again, the GUI can serve as a reference.
--RJH