Other Parts Discussed in Thread: DAC38J84
Team-
Customer would like to drive IF port of TRF3722 single-ended, i.e. one side of the differential input drive, while the other side is terminated.
Certainly this will impact certain performance parameters; that would be expected.
Want to know if this will work with reduced performance and if AC or some sort of DC bias should be placed on the unused/terminated input.
From the data sheet it appears that a common mode of 0.25V should be on BBQ_P/BBQ_N. Is it OK to bias this with a voltage divider having 0.25V output and output impedance of ~50 Ohms to terminate the BBQ_N port? We would then drive BBQ_P with single-ended 50 Ohm system.
Thanks, Best, Steve