This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7920EVM: Bring up in Latte

Part Number: AFE7920EVM
Other Parts Discussed in Thread: TSW14J56EVM

Hi,

I just recently got the AFE7920EVM delivered. 

I would like to use the AFE7920EVM stand-alone, i.e. without the TSW14J56EVM as mentioned in  the EVM user guide.

I've powered the AFE7920EVM from a stable 5V source, D5-D6-D7-D8-D9 all lit.

I've conntected the EVM to a PC running Latte, D10 lit (dim).

Latte does not seem te be aware of any EVM connected, there isn't a single script visible in Latte that I could try to run.

Is the issue with the EVM or the Latte installation?

Thanks.