This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82: # un bits and # en bit

Part Number: DAC38RF82


Like to know the meaning of # un bits and # en bit in Table 10 to Table 27. Thanks.

  • new2day,

    #un means number of unencoded bits

    #en means number of encoded bits

     

    However, both are running (accumulating) totals as you read from left to right.

     

    So the first 4 unencoded bits are labeled with #un=4.  The next four are labeled with #un=8. If the frame was longer, the next nibble would have #un=12, then 16, etc. (incrementing by 4).

    The #en labels would go 5, 10, 15, 20, 25, …

     

    Regards,

     

    Jim