This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF89: DAC Fullscale Output Current

Part Number: DAC38RF89

DAC38RF89 have two DACs,we want to change the DAC1's Fullscale Output Current. But there is only one register(page4,0x0D) to set the current. When change the value, the DAC2 is changed too.

How can change the two DAC‘s Fullscale Output Current  separately? For example, DAC1 is 30mA, and DAC2 is 40mA.