Hi, I am new to this topic, so my questions might be sound primitive but answers are very important;
1- are the registers values of ;
Type of transfers,
Type of register,
PATABLE & FIFO's,
Command strobes,
Status registers, and
CC1101 configuration registers
are mandatory in the code before the actual configured registers values exported from the SmartRF Studio?
2- I have two CC1101 modules with D-SUN 433 MHz printed on them, does that mean they are pre-configured with
with 433 MHz band? and the band can be changed to a different band for example 313 MHz via SmartRF Studio?
3- Obviously the modules after programming, will not work on their own without Micro controller unit, the question is
after interfacing the module to SmartRF Studio to get the registers configuration, will the same registers be added to the code?
or export the registers as a file and then add it to the code?
Thanks in advance