Dear Sir,
I have to generate the two chirp signals simultaneously from each DAC of the Dual DAC chip: DAC38RF82. The Chirp Signals are 1.92GHz ± 800MHz and 1.92GHz ± 950MHz using a DAC Clock frequency of maximum 9GHz.
Kindly confirm if this is possible, If yes, what is spurious and harmonic supressions levels.
If not possible, what is maximum bandwidth we can achieve for the both the chiro generations in DAC38RF82.
Regards,
Aruna Neeli