Other Parts Discussed in Thread: AFE7444, , TSW14J57EVM
Hello,
We downloaded the reference design to use the EVM with the KCU105.
The JESD interface is operated at 7.372Gbps and the corresponding DAC sampling rate is mentioned as 368.64MSps (limiting the signal BW to 180MHz).
Our signal bandwidth is around 500MHz.
May I ask you to please help us with the following:
1) What changes need to be done in the reference design to digitize a 500MHz BW signal and then reproduce the same using the DAC (as a first test).
Regards,