DAC38RF82: DAC38RF82

Prodigy 10 points

Replies: 1

Views: 31

Part Number: DAC38RF82

Hellow, when I used SPI to program DAC38RF82, the odd registers of the address read and write normally, but the even registers of the address read and write goes error.  If you known , thanks for your help.

1 Reply

  • Guru 64670 points

    Zhang,

    Make sure you are issuing a hard reset to the DAC after power and clocks are present. You may have to probe the SDIO, SEN and SCLK with a scope and verify the timing and signal levels with respect to the data sheet. The only way I could see this happening is for address bit 0 to be stuck at "1". Is the data being sent one clock early/late with respect to SDEN going low by any chance?

    Is this issue with writes/reads to all four pages?

    Regards,

    Jim