Hi everyone,
I am currently studying the reference design KCU105 AFE74xx XCVR 2x44210. The reference Vivado project is implemented on Vivado v2016.1. However I would like to port it to Vivado v2018.2 and started building the block design from scratch. I see some of the IPs are not present in the IP repository of Vivado v2018.2.
After searching through reference design, I was able to add the following IPs in Vivado v2018.2, by adding the path of repository directory 'repository_0' from the reference design.
1.iobufs_ti_v1_0
2.leds_v1_0
However, the following IP (source) is still missing
1.transport_layer_afe768x_44210_0
Does ti provide support for this? How can I obtain this IP so I can complete re-building the block design on Vivado 2018.2?
Can someone help me with this?
Thanks in advance,
-Chandrasekhar DVS