Other Parts Discussed in Thread: ADC32RF80, , LMK04828
Hello
I request an ini file of HSCDpro to test the mod below.(ADC32RF80_LMF_8821_alternate.ini)
Could you provide the ADC32RF80_LMF_8821_alternate.ini file?
Best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I request an ini file of HSCDpro to test the mod below.(ADC32RF80_LMF_8821_alternate.ini)
Could you provide the ADC32RF80_LMF_8821_alternate.ini file?
Best regards
Have you tried with the regular INI (the one without "alternate") which is included with HSDC Pro? It's called "ADC32RF80_LMF_8821" and that should work. ADC32RF80_LMF_8821.ini
Hi Louis,
The HSDC Pro error you showed is typically seen when the reference clock from ADC EVM to the TSW14J56 board is incorrect. The ADC EVM GUI shows that you are configuring it for internal clocking at 2457.6Msps and a DDC factor of 20x. That will result in an output data rate of 122.88Msps (2457.6/20). But in HSDC Pro data, the data rate is set to 307.2M which doesn't match.
Can you review the sampling clock frequency, DDC and output data rate to make sure they are consistent?
Regards,
satish.
Hi satish
Thanks for your support.
I tested it with data rate of 122.88Msps, but the result was the same error.
When the DDC factor of 16x and ADC32RF80_LMF_8821.ini is used, it operates normally.
Could you test the DDC factor of 20x with ADC32RF80EVM?
Best regards
Hi Louis,
I've tested this mode on my bench earlier and it had worked without any issues. The issue here is probably incorrect FPGA reference clock frequency. You can rule this out by clicking on the "LMK04828" tab in the GUI and checking the "DCLK Divider" under the "CLKout 0 and 1" group. You must check this after programming the EVM. The LMK VCO frequency divided by this number should match the reference clock frequency expected by the TSW14J56 board. The expected frequency is shown on a pop-message in HSDC Pro when you configure the ADC tab of HSDC Pro.
In your screenshots, you seem to be using an external clock source to clock the ADCEVM. In that case, you'll also have to provide a copy of the ADC clock to LMK (SMAs J5 and J7).
I'll test again on my bench when I get a chance.
regards,
satish.
Hi Louis,
I have found the problem and the fix. The reference clock to the FPGA in the mode you are trying to configure is beyond what LMK can generate. The fix is to use a different FPGA reference clock. Please use the attached INI file, which uses SerDes_rate/10, instead of the typical SerDes_rate/40.
You'll also have to modify the LMK clock divider (to 10) after you configure the EVM. You should be able to capture with these changes. Attached are 2 files for your reference.
Regards,
satish.