Other Parts Discussed in Thread: LM27761,
Hi
In my board DAC38RF83 current consumption at VEE18N power rail is 340 mA. Which is to high, relative to datasheet. Power supply schematic is the same as in EVB. I measured it trough small value serial resistor at the output of LM27761. The DAC outputs are terminated to +1.8V trough 56nH and connected to TCN2-14+ balun (AC coupled). The current at EVB is 150 mA, both DACs not configured.
What could be the cause of such a high current?