I config DAC38RF89's JESD204B as fallowing.
It has two real input. One use DACA, the other use DACB.
When I initial DAC38RF89, the two DACs output has a phase difference,t1(two channels data is the same); if I re-initial DAC38RF89,the phase difference sometimes becomes t2 and sometimes it doesn't change.
I want to know the reason? And how can the phase difference be fixed to 0?