This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7769EVM: AFE7769 AUX ADC read out

Part Number: AFE7769EVM
Other Parts Discussed in Thread: AFE7769

HI all

We use AFE7769 onchip AUX 12bit SAR ADC to sample low-speed signal like PA temperature. And We use function auxAdcInSel and readAuxAdc to finish the job.

We test INP=VREF/2, INM=AVSS and INP=AVSS, INM=VREF/2, the conversion result is correct.

But if seting INP=AUX5, INM=AVSS(the input voltage is 0.4V on GPIOD2), the conversion result is only 2080,which is 0.02V. Just like the signal doesn't come in.

I try to bypass the the input buffer,disable the GPIO pullup and set GPIO for analog input.

I don't know whether the operation is correct because the datasheet use GPIOB/C/D/E but the register map use GPIO0~79, but doesn't tell the mapping relationship.

And the register map also mentioned a crossbar selection which refer to a separate xls file. how can we download the crossbar file and gpio mapping information?

TKS!!