Other Parts Discussed in Thread: ISO1541
Hello,
We try to develop a system which is related to sense capacitance between a custom designed capasitance circuit and grounded plate.
We have a servo system to set height of the system which we try to measure its height with FDC1004.
We have some connection problem between i2c and microprocessor.
We can measure the capacitance when we make run them on the bench without servo system. But when we connect the capacitive sensing system to servo system, the connection between sensor and microprocessor is broken. We tried to disconnect motor chasis and capacitive sensor ground, the problem was solved partly. Until the sensor touch the plate, everything is okay but after the sensor touch the plate, i2c connection is broken.
Do you have any idea about the problem? Do we do something wrong? What can we do to solve this?
Thanks.
Ahmet