Hello,
I have a question regarding the DRV5032FADBZR used with Vcc = 3,7V.
In the Datashett Icc(PK) is only specified over the Range of 1,65V < Vcc < 5,5V at max 2,7 mA
and Icc(AVG) at 3V Vcc with 1,6 µA.
How do these Values look with Vcc = 3,7 ?
Regards Andreas