Other Parts Discussed in Thread: TIPD205, , , OPA320, TIDA-00218, DRV5053, DRV5055
Hi,
I want to measure DC current of power-battery,the current will be up to 800A, does TI have a solution?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Zehua,
A cheaper way is using one of our linear hall sensors and use the B = (µ0*I) /(2*π*r) to calculate the current at a specific distance for a wire. You could use a concentrator like the TIDA-00218 but that may saturate the sensor. You would need to calibrate the hall sensor as they are not as accurate as a fluxgate device.
Hi Javier,
TIDA-00218 is used to measure AC current, can it measure DC current up to 800A? Do you have any app-notes on this application?
Thanks very much!