Hi,
I have some questions regarding the DRV425 device.
My intended usage is to use several of these sensors to estimate the 3D position of a permanent magnet with respect to the sensor location. The target is to detect this magnet within a range from a few mm up to several (5+) cm. A rudimentary FEM simulation tells us that we would like to measure down to ~ 2uT at our sensor location and it is possible that the sensor will experience fields up to 200mT. We would like a measurement BW of ~100Hz.
I have a few questions about some situations that may apply to my product and I hope you can provide me with some more insights. My apologies in advance if things are clearly stated in the datasheet or have already been explained in the forum, and I have failed to notice them!
I believe that noise and temperature drifts using this sensor and a suitable ADC will remain below 2uT. I therefore think my biggest obstacle at the moment is initial offset and hysteresis.
Q: The worst case sensor offset is +/-8uT. Can you say something about the long term stability of this offset? In other words; If I compensate for this offset once after production, will this compensation be valid over the intended life-time of my instrument (several years) assuming conditions remain the same? Or do I need yearly/monthly/… calibration/adjustment.
Q: You mention a typical hysteresis of 1.4uT when a -/+10mT sweep is applied. Is there an easy answer to what causes this hysteresis? Does this number change when we apply +/-200mT? Is there some predictability to this hysteresis, if we can for instance predict the actual field strength and direction at the location of the sensor?
Q: If I place the sensor in a 2mT homogeneous field that is in the x-direction. What can I expect from the sensors sensitive in the y and z direction? Is there some crosstalk or is the sensor absolutely insensitive in the directions perpendicular to the sensitivity axis. (and what if this field is 200mT?)
Thank you in advance for your reply,
With kind regards,
Jasper Keuning