Other Parts Discussed in Thread: DRV421, DRV401
Hi! javier!
the problems in DRV421 were resolved ,but it was not automotive.so i focus on 401-Q1.
according to datasheet, the probe core reaches saturation at a current of 28mA. i have a question, if i have two probe core with different materails, one reaches saturation at 10mA, another reaches saturation at 70mA, if i use these probe cores ,what will happen? the probe core saturation >28mA or <28mA, which is better ? and if i use the probe core saturation at 70mA, is ok?what the impact of that ? the accuracy, the response speed or any other influence?
thank you ! Best regards!