Dear Jose-san,
In the past, Fukasawa received Jose-san special support on the humidity accuracy of HDC 1080.
We are continuing QA with customers, but we have not solved it.
Please let me ask a question again.
<Situation>
An HDC 1080 is mounted on a mass production board of a customer.
This board is called a board A.
However, humidity accuracy errors occurred on some board A.
Therefore, exactly the same size as board A,
board B composed of the same parts was prepared.
The customer has identified the cause by comparing board A and board B.
※ Board size = 0.4 cm × 1.3 cm
Configuration = HDC 1080 + 1 capacitor only
However, an error of + 5% steadily occurs in the humidity accuracy
measured on the board B.
Also, as a result of allowing the board B to reflow again and then leaving it,
it was possible to confirm the result that the accuracy recovered.
(Reflow is recommended only once. Customer is known)
<Question>
① We don't understand why the difference between board A and B occurs although
both of their production conditions are same.
Could you list possible cause?
② If the reflow temperature is low, is there a possibility of an accuracy error of 5%?
Because accuracy restoration was confirmed when re-reflow was applied.
Best,Regars.
Fukazawa