Hi all,
how can I know when the HDC2010 sensor is self-breaking? For example, if the resistance sensor of the temperature is in CC or in CA, what are the output signals on pin 3?
The chapter "7.3.2 Heater" in the datasheet tell: "The heater is an integrated resistive element that can be used to test the sensor or to drive condensation off the
sensor...."
Can I use this component to know when the sensor is self-breaking?
Are there others parameters to check the correct function?
Thanks a lot
Francesco