Other Parts Discussed in Thread: LDC1000EVM
I'm evaluating the LDC1000EVM now with using the coil which I made.
The coil is connected to the coaxial cable(3m), and the coaxial cable connected to the LDC1000.
The coil has approx 19uH and 3.72ohm with including the coaxial cable.
I refer to the EVM Quick Start Guide, and determin the C value(470pF) and the frequency(1333kHz).
After these parameters(also Rp min and max) have been set on the LDC GUI software, it shows the proximity data change when the target distance changes. This means the system seem to work correctly.
But if I touch the coaxial cable, the proximity data changes.
I understand C value has been changed by touching the coaxial cable, this results in the proximity data changes.
Question:
Does anyone have any ideas or any clues to avoid(or reduce) this kind of cable issues?
Should these type sensor not be used with the cable?
Please advise.