Using the LDC1312 EVM and GUI, whatever I do, I only get 4 bit data, or 4 bit data plus error bit(s). I looked at the I2C data and reading from the odd data address always gives 0xff. This is even using the on-board inductors.The coil is operating at around 2MHz, and I have tried selling the clock dividers to reduce the reference from 40MHz without success.
On one setting (divide by 10) I get the watchdog timeout error. I can find no documentation to tell me what this means.
Charles