This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614 Interference for cable

Guru 16770 points

Hi

We are facing the problem of interference in the following situations.

If human body comes close to the cable, the measurements are not stable.

Do you have solutions to avoid this?

regards

  • Hello na na,

    by moving your hands close to the cable, you are changing its capacitance, which alters the oscillation frequency. Note that both inductance changes and capacitance changes shift the oscillation frequency which is measured by the LDC, and it may therefore be difficult to distinguish between the two effects.

    Here are some things you could try:

    1. Reducing cable length is obviously best, but I know it isn't always possible. Please make sure that long cables are securely attached (glued) to the housing of your system so that they don't bend during operation and cause a capacitance change.  

    2. Are you using a shielded cable? I recommend UTP cable (unshielded twisted pair), as the shield has a lot of capacitance itself, which can be affected by the environment. 

    3. Use a larger Csensor capacitor. By increasing the sensor capacitor, the cable capacitance will appear small by comparison, and its effect will be reduced.

  • Let me also add that the observed noise is 500 codes out of 19,000,000, or 0.0026%.

    The main question is how does it compare vs your signal?

  • Hi Ben
    Thank you for your reply.

    We'll check your advice and try.

    regards
  • Hi Evgeny

    Thank you for your comment also.

    The measured data as signal is also 500 code because the target is very small.

    regards
  • You're welcome. I hope you managed so resolve the issue.